-
PFA Needle Valves
CAUTION: PFA needle valves do not typically exhibit the same positive shutoff feel as metal valves.
-
Installation Instruction, Bar Handle to 40 Series Valve
Note orientation of the directional handle. Bar handle must be installed pointing in the same direction as the removed handle; Loosen set screw; Remove current handle. Also remove the handle stop insert when applicable.
-
40 Series Optional Handles
If the valve handle is removed, please note its orientation; When reinstalled, the handle must be in the same orientation.
매장 위치로 구입 가능한 제품 보기
시간