Результаты поиска по «{0}»
Ведете поиск продукции, связанной с:
В местном авторизованном центре продаж и сервисного обслуживания Swagelok могут быть дополнительные варианты.
-
PFA Needle Valves
CAUTION: PFA needle valves do not typically exhibit the same positive shutoff feel as metal valves.
-
Installation Instruction, Bar Handle to 40 Series Valve
Note orientation of the directional handle. Bar handle must be installed pointing in the same direction as the removed handle; Loosen set screw; Remove current handle. Also remove the handle stop insert when applicable.
-
40 Series Optional Handles
If the valve handle is removed, please note its orientation; When reinstalled, the handle must be in the same orientation.
Наличие изделий по местоположению склада
часов