text.skipToContent text.skipToNavigation

Search Results for "{0}"

Are you looking for product listings related to:

Your local authorized Swagelok sales and service center may have additional options.

You're Filtering By:
  • Engineering Services
Clear All Filters
Filter By:
Подбор изделий с учетом требований безопасности:

Для того чтобы проектировщик системы и пользователь могли гарантированно выполнить подбор изделий с учетом требований безопасности, необходимо принять в рассмотрение дизайн системы и полный каталог продукции. При выборе изделий следует принимать во внимание всю систему в целом, чтобы обеспечить ее безопасную и бесперебойную работу. Соблюдение назначения устройств, совместимости материалов, надлежащих рабочих параметров, правильный монтаж, эксплуатация и обслуживание являются обязанностями проектировщика системы и пользователя.

⚠ ПРЕДУПРЕЖДЕНИЕ: Запрещается совместное использование и замена продуктов или компонентов Swagelok, на производство которых не распространяются отраслевые стандарты проектирования (в том числе торцевых соединений трубных обжимных фитингов Swagelok), продуктами или компонентами других производителей.

  • Oil & Gas Tubing System Training

    The Swagelok ® Tubing System Training Program, Oil and Gas The Swagelok ® Tubing System Training Program, Oil & Gas, is a globally standardized two-day workshop designed to address the JIP33 S-716 requirement and give your team thorough instruction on industry best practices for ensuring high-int...

  • API Plan 75 Condensing Leakage Collection

    < Back to Between Seal Plans API Plan 75 collects leakage from the inboard seal in applications where normal process fluid leakage can condense between the seals at ambient temperatures. In this arrangement, a reservoir is connected to the containment seal drain port on the gland. Condensed leakag...

  • API Plan 76 Noncondensing Leakage Collection

    API Plan 76 collects leakage from the inboard seal in applications where normal process fluid leakage does not condense between the seals at ambient temperatures. In this piping plan, gaseous leakage from the inboard seal exits through the containment seal vent port in the gland. The orifice creates...

  • API Plan 72/76 Buffer Gas and Noncondensing Leakage Collection

    This panel is a combination of API Plan 72 and Plan 76. The Plan 72 side supplies a buffer gas from an external source between the inboard and outboard faces of a dual seal. For reliable operation, gas seals require a constant supply of clean, dry gas, typically nitrogen. The seal support panel cont...

  • Process Side Plans

    < Back to Mechanical Seal Support Systems Seal Support System Process Side Plans Seal Plan Kits Most Swagelok-built process side plans for seal support are available as seal plan kits. Each kit containseverything needed for proper installation, including an engineered drawing, making it simple t...

  • API Plan 11 Flush

    < Back to Process Side Plans API Plan 11 recirculates flow from a high‐pressure section of the pump, typically the discharge piping, through a flow control orifice to the seal. Plan 11 is the default flush plan for most pumps. API Plan 11 Kit components shown solid and include some optional c...

  • Capital Projects Product Selection Guide

    Global Construction Product Selection Guide Managing Your Capital Project Any large-scale construction project is inherently difficult. Thousands of people are involved, competition is aggressive, logistics are complicated, spending approvals can come slowly, and there is a constant threat of p...

  • API Plan 12 Flush with Strainer

    API Plan 12 recirculates flow from a high‐pressure section of the pump, typically the discharge piping, through a flow control orifice to the seal. In order to remove particulate in the flush stream and prevent clogging, flow passes through a strainer placed prior to the flow control orifice. The ad...

  • API Plan 13 Flush from Chamber to Suction

    API Plan 13 recirculates flow from the seal chamber to the suction side of the pump. This plan is common for vertical pumps. API Plan 13 Kit components shown solid and include some optional components. This plan: Removes heat and flushes particulate from the seal chamber Allows the...

  • API Plan 14 Flush, Combination of Plans 11 & 13

    API Plan 14 combines Plan 11 and Plan 13. Flow is recirculated from the pump discharge into the seal chamber and from the seal chamber to the pump suction. Fluid flow is increased since the seal chamber is continuously vented, leading to higher cooling capacity. API Plan 14 Kit components show...

This process may take several minutes. Please be patient and remain on the page.