Search Results for "{0}"
Are you looking for product listings related to:
Your local authorized Swagelok sales and service center may have additional options.
-
API Plan 11 Flush
< Back to Process Side Plans API Plan 11 recirculates flow from a high‐pressure section of the pump, typically the discharge piping, through a flow control orifice to the seal. Plan 11 is the default flush plan for most pumps. API Plan 11 Kit components shown solid and include some optional c...
-
API Plan 12 Flush with Strainer
API Plan 12 recirculates flow from a high‐pressure section of the pump, typically the discharge piping, through a flow control orifice to the seal. In order to remove particulate in the flush stream and prevent clogging, flow passes through a strainer placed prior to the flow control orifice. The ad...
-
API Plan 13 Flush from Chamber to Suction
API Plan 13 recirculates flow from the seal chamber to the suction side of the pump. This plan is common for vertical pumps. API Plan 13 Kit components shown solid and include some optional components. This plan: Removes heat and flushes particulate from the seal chamber Allows the...
-
API Plan 14 Flush, Combination of Plans 11 & 13
API Plan 14 combines Plan 11 and Plan 13. Flow is recirculated from the pump discharge into the seal chamber and from the seal chamber to the pump suction. Fluid flow is increased since the seal chamber is continuously vented, leading to higher cooling capacity. API Plan 14 Kit components show...
-
API Plan 21 Cooled Flush
API Plan 21 adds a cooler to Plan 11 for applications requiring better control of flush vapor margin. Flow is routed from the discharge side of the pump through an orifice and a cooler before being returned to the seal chamber. API Plan 21 Kit components shown solid and include some optional co...
-
API Plan 22 Cooled Flush with Strainer
API Plan 22 adds a strainer to Plan 21. Flow is routed from the discharge side of the pump, through a strainer, an orifice, and a cooler before being returned to the seal chamber. The addition of pressure gauges on either side of the strainer allows the strainer to be monitored for servicing. In dry...
-
API Plan 23 Cooled Flush, Recirculated through Seal Chamber
< Back to Process Side Plans API Plan 23 utilizes a circulation device, typically a pumping ring, to route the fluid from the seal chamber through a cooler before returning the cooled fluid to the seal chamber. A throat bushing isolates the cooled seal chamber flush fluid from the hotter pumped li...
-
API Plan 31 Flush with Cyclone Separator
API Plan 31 is used to remove solids from the flush stream by incorporating a cyclone separator into the flush tubing. Flow is routed from the discharge side of the pump through the cyclone separator. Clean flush fluid leaving the separator is routed to the seal chamber while fluid containing the so...
-
API Plan 41 Cooled Flush with Cyclone Separator
API Plan 41 is a cooled version of Plan 31. Solids are removed from the flush fluid by incorporating a cyclone separator. Flow is routed from the discharge side of the pump through the cyclone separator. Clean flush fluid leaving the separator is routed through a cooler before being returned to the ...
-
Mechanical Seal Design Principles & Basics
Better by Design: Swagelok Seal Support Systems Swagelok leverages deep fluid system expertise to design and construct simple-to-configure, easy-to-maintain,and safe-to-operate seal support systems. If you are tasked with keeping rotating equipmentonline and operating efficiently, you will find tha...