text.skipToContent text.skipToNavigation

Search Results for "{0}"

Are you looking for product listings related to:

Your local authorized Swagelok sales and service center may have additional options.

You're Filtering By:
  • Engineering Services
Clear All Filters
Filter By:
Safe Product Selection

The complete catalog contents must be reviewed to ensure that the system designer and user make a safe product selection. When selecting products, the total system design must be considered to ensure safe, trouble-free performance. Function, material compatibility, adequate ratings, proper installation, operation, and maintenance are the responsibilities of the system designer and user.

⚠ Warning: Do not mix/interchange Swagelok two-ferrule tube-fitting end connection components (or other products not governed by industrial design standards) with those of other manufacturers.

  • Sampling System Problem Solving and Maintenance (SSM)

    Sampling System Problem Solving and Maintenance Training Swagelok ®  Sampling System Problem Solving and Maintenance (SSM) training courses will teach youhow to troubleshoot a variety of common sampling system issues from the process line throughsample disposal. Attendees will learn how to troubles...

  • Webinars

    Increase Your Fluid System Knowledge Through Swagelok Webinars Keep your fluid system design, operation, and maintenance skills up to date by attending or watching Swagelok webinars on demand. Our subject-matter experts regularly help industrial professionals around the world better understand ev...

  • API Plan 65A Leakage Collection with Reservoir

    API Plan 65A monitors leakage in a single seal arrangement. Connected to the drain port on the gland, a reservoir collects normal leakage and is constantly open to drain. In the event of a seal failure, an orifice fitting on the outlet of the system allows a level transmitter to trigger an alarm due...

  • API Plan 65B Leakage Collection with Reservoir

    API Plan 65B monitors leakage in a single seal arrangement. Connected to the drain port on the gland, a reservoir is allowed to collect normal leakage. A level transmitter on the reservoir triggers an alarm in the event of excessive leakage. A valve on the outlet side of the reservoir is typically l...

  • Between Seal Plans

    < Back to Mechanical Seal Support Systems Seal Support System Between Seal Plans Seal Plan Assemblies Swagelok-built between seal plans for seal support are available as seal plan assemblies only. Optionsand configurations not listed in the ordering numbering structure are also available, and se...

  • API Seal Plan 52 Buffer Fluid Seal Pot

    < Back to Between Seal Plans API Seal Plan 52 utilizes a reservoir and circulates an unpressurized buffer fluid between the inboard and outboard seals. To provide positive circulation through the support system and into the seal, a pumping ring is employed. Frictional losses in the buffer fluid in...

  • API Plan 53A Barrier Fluid Seal Pot Pressurized by Nitrogen

    API Plan 53A utilizes a reservoir and circulates a pressurized barrier fluid between the inboard and outboard seals. The typical source of pressurization is plant nitrogen. The reservoir should be set at least 20 psi (1.3 bar) above maximum seal chamber pressure. This is to ensure that leakage acros...

  • API Plan 53B Barrier Fluid Pressurized by Bladder Accumulator

    API Plan 53B circulates a pressurized barrier fluid between the inboard and outboard seals. The source of pressurization is a bladder accumulator. Plan 53B has the advantage of not allowing gas absorption into the barrier fluid which may allow for operation at higher pressures than Plan 53A. Barrier...

  • API Plan 53C Barrier Fluid Pressurized by Piston Accumulator

    API Plan 53C circulates a pressurized barrier fluid between the inboard and outboard seals. The source of pressurization is a piston accumulator. Plan 53C is preferred for applications where the seal chamber pressure may vary during pump operation. A sensing line is typically run from the seal chamb...

  • API Plan 54 Barrier Fluid Pressurized by External System

    API Plan 54 is a custom engineered system that delivers a pressurized barrier fluid to the seal chamber. The barrier liquid is circulated to and from the seal chamber via a pump located on an external reservoir. This fluid is maintained at a pressure greater than that found in the seal chamber. A Pl...

This process may take several minutes. Please be patient and remain on the page.