Search Results for "{0}"
Are you looking for product listings related to:
Your local authorized Swagelok sales and service center may have additional options.
-
API Plan 54 Barrier Fluid Pressurized by External System
API Plan 54 is a custom engineered system that delivers a pressurized barrier fluid to the seal chamber. The barrier liquid is circulated to and from the seal chamber via a pump located on an external reservoir. This fluid is maintained at a pressure greater than that found in the seal chamber. A Pl...
-
API Plan 11 Flush
< Back to Process Side Plans API Plan 11 recirculates flow from a high‐pressure section of the pump, typically the discharge piping, through a flow control orifice to the seal. Plan 11 is the default flush plan for most pumps. API Plan 11 Kit components shown solid and include some optional c...
-
API Plan 14 Flush, Combination of Plans 11 & 13
API Plan 14 combines Plan 11 and Plan 13. Flow is recirculated from the pump discharge into the seal chamber and from the seal chamber to the pump suction. Fluid flow is increased since the seal chamber is continuously vented, leading to higher cooling capacity. API Plan 14 Kit components show...
-
Capital Projects Product Selection Guide
Global Construction Product Selection Guide Managing Your Capital Project Any large-scale construction project is inherently difficult. Thousands of people are involved, competition is aggressive, logistics are complicated, spending approvals can come slowly, and there is a constant threat of p...
-
API Plan 13 Flush from Chamber to Suction
API Plan 13 recirculates flow from the seal chamber to the suction side of the pump. This plan is common for vertical pumps. API Plan 13 Kit components shown solid and include some optional components. This plan: Removes heat and flushes particulate from the seal chamber Allows the...
-
API Plan 55 Buffer Fluid Circulated by External System
API Plan 55 is a custom engineered system that delivers an unpressurized buffer fluid to the seal chamber. The buffer liquid is circulated to and from the seal chamber via a pump located on an external reservoir. A Plan 55 can contain filters, coolers, and other components that are selected accordin...
-
API Plan 72 Buffer Gas
API Plan 72 supplies a buffer gas from an external source between the inboard and outboard seals. For reliable operation, gas seals require a constant supply of clean, dry gas, typically nitrogen. The seal support panel contains a coalescing filter to remove any moisture and particulate present in t...
-
API Plan 74 Barrier Gas
< Back to Between Seal Plans API Plan 74 supplies a pressurized barrier gas from an external source between the inboard and outboard seals. For reliable operation, dual pressurized gas seals require a constant supply of clean, dry gas, typically nitrogen. The seal support panel contains a coalesci...
-
API Plan 75 Condensing Leakage Collection
< Back to Between Seal Plans API Plan 75 collects leakage from the inboard seal in applications where normal process fluid leakage can condense between the seals at ambient temperatures. In this arrangement, a reservoir is connected to the containment seal drain port on the gland. Condensed leakag...
-
API Plan 76 Noncondensing Leakage Collection
API Plan 76 collects leakage from the inboard seal in applications where normal process fluid leakage does not condense between the seals at ambient temperatures. In this piping plan, gaseous leakage from the inboard seal exits through the containment seal vent port in the gland. The orifice creates...