text.skipToContent text.skipToNavigation

Search Results for "{0}"

Are you looking for product listings related to:

Your local authorized Swagelok sales and service center may have additional options.

You're Filtering By:
  • Engineering Services
Clear All Filters
Filter By:
Safe Product Selection

The complete catalog contents must be reviewed to ensure that the system designer and user make a safe product selection. When selecting products, the total system design must be considered to ensure safe, trouble-free performance. Function, material compatibility, adequate ratings, proper installation, operation, and maintenance are the responsibilities of the system designer and user.

⚠ Warning: Do not mix/interchange Swagelok two-ferrule tube-fitting end connection components (or other products not governed by industrial design standards) with those of other manufacturers.

  • Hydrogen Tubing System Training

    The Swagelok ® Tubing System Training Program, Hydrogen Applications One of the most formidable challenges in the development of safe, dependable, and leak-tight hydrogen fluid systems is the nature of hydrogen itself. Hydrogen is a small-molecule gas that can easily escape through the tiniest ...

  • Materials Science

    Training in Materials Science Swagelok ®  Materials Science training courses teach you how to choose the right corrosion-resistant materials to help you keep your fluid systems leak-tight and operating efficiently. Through this course, you will learn which specific alloys resist corrosion and how t...

  • Leak Detection Case Studies

    Swagelok ® Compressed Gas Leak Detection Services Customer Success Stories Every day, experienced Swagelok fluid system specialists and field engineers  with deep technical and application expertise consult with customers in diverse industries across the globe on fluid system design, installatio...

  • Hose Management

    Swagelok ® Hose Advisory Services: Helping You Get More from Your Hoses   Eliminate a variety of hose-related issues that cause safety concerns , unplanned downtime, low product yield, or costly part replacements through Swagelok ® hose advisory services. Experienced Swagelok hose advisors will...

  • Advanced Tube Bending

    Training in Advanced Tube Bending It has often been said that tube bending is an art, not a science. While it is true that bent tube can take on an artistic appearance  when done well,  the real art of bending  tubing lies in the operator’s ability toovercome the variables inherent to the bending ...

  • Design and Assembly Services

    Take the Building and Testing of Fluid System Assemblies Off Your To-Do List If you’re short on trained personnel or simply short on time, Swagelok-trained technicians can provide an extra set of hands by fabricating your fluid system assemblies for you. You will receive a professionally designed, ...

  • Atmospheric Side Plans

    < Back to Mechanical Seal Support Systems Seal Support System Atmospheric Side Plans Seal Plan Kits Swagelok-built atmospheric side plans for seal support are available as seal plan kits only. Each kitcontains everything needed for proper installation, including an engineered drawing, making it...

  • API Plan 51 Quench from Reservoir

    API Plan 51 is a quench system for use on the atmospheric side of a single seal. This system acts as a dead-ended reservoir for a fluid. API Plan 51 Kit contents shown solid and include some optional components. This plan: Prevents icing on the atmospheric side of the seal Is typic...

  • API Plan 62 Quench from External Source

    API Plan 62 delivers an external quench fluid to the atmospheric side of the seal. A typical application in a refinery is the prevention of coking on seal faces in hot hydrocarbon service by employing a steam quench. Nitrogen or clean water may also be used to quench or cool and clean the atmospheri...

  • API Plan 65A Leakage Collection with Reservoir

    API Plan 65A monitors leakage in a single seal arrangement. Connected to the drain port on the gland, a reservoir collects normal leakage and is constantly open to drain. In the event of a seal failure, an orifice fitting on the outlet of the system allows a level transmitter to trigger an alarm due...

This process may take several minutes. Please be patient and remain on the page.