Search Results for "manifolds"
Are you looking for product listings related to: manifolds
Your local authorized Swagelok sales and service center may have additional options.
-
API Plan 13 Flush from Chamber to Suction
API Plan 13 recirculates flow from the seal chamber to the suction side of the pump. This plan is common for vertical pumps. API Plan 13 Kit components shown solid and include some optional components. This plan: Removes heat and flushes particulate from the seal chamber Allows the...
-
API Plan 51 Quench from Reservoir
API Plan 51 is a quench system for use on the atmospheric side of a single seal. This system acts as a dead-ended reservoir for a fluid. API Plan 51 Kit contents shown solid and include some optional components. This plan: Prevents icing on the atmospheric side of the seal Is typic...
-
API Plan 65A Leakage Collection with Reservoir
API Plan 65A monitors leakage in a single seal arrangement. Connected to the drain port on the gland, a reservoir collects normal leakage and is constantly open to drain. In the event of a seal failure, an orifice fitting on the outlet of the system allows a level transmitter to trigger an alarm due...
-
API Plan 65B Leakage Collection with Reservoir
API Plan 65B monitors leakage in a single seal arrangement. Connected to the drain port on the gland, a reservoir is allowed to collect normal leakage. A level transmitter on the reservoir triggers an alarm in the event of excessive leakage. A valve on the outlet side of the reservoir is typically l...
-
API Plan 14 Flush, Combination of Plans 11 & 13
API Plan 14 combines Plan 11 and Plan 13. Flow is recirculated from the pump discharge into the seal chamber and from the seal chamber to the pump suction. Fluid flow is increased since the seal chamber is continuously vented, leading to higher cooling capacity. API Plan 14 Kit components show...
-
API Plan 11 Flush
< Back to Process Side Plans API Plan 11 recirculates flow from a high‐pressure section of the pump, typically the discharge piping, through a flow control orifice to the seal. Plan 11 is the default flush plan for most pumps. API Plan 11 Kit components shown solid and include some optional c...
-
API Plan 21 Cooled Flush
API Plan 21 adds a cooler to Plan 11 for applications requiring better control of flush vapor margin. Flow is routed from the discharge side of the pump through an orifice and a cooler before being returned to the seal chamber. API Plan 21 Kit components shown solid and include some optional co...
-
API Plan 23 Cooled Flush, Recirculated through Seal Chamber
< Back to Process Side Plans API Plan 23 utilizes a circulation device, typically a pumping ring, to route the fluid from the seal chamber through a cooler before returning the cooled fluid to the seal chamber. A throat bushing isolates the cooled seal chamber flush fluid from the hotter pumped li...
-
API Plan 62 Quench from External Source
API Plan 62 delivers an external quench fluid to the atmospheric side of the seal. A typical application in a refinery is the prevention of coking on seal faces in hot hydrocarbon service by employing a steam quench. Nitrogen or clean water may also be used to quench or cool and clean the atmospheri...
-
API Plan 12 Flush with Strainer
API Plan 12 recirculates flow from a high‐pressure section of the pump, typically the discharge piping, through a flow control orifice to the seal. In order to remove particulate in the flush stream and prevent clogging, flow passes through a strainer placed prior to the flow control orifice. The ad...